Depends on the BEC you are connecting to the servo rail. If you like to run servo's you need to connect a BEC/5V supply to the servo rail input. The FMUK66 is not supplying power to the servo-rail.
Depends on the BEC you are connecting to the servo rail. If you like to run servo's you need to connect a BEC/5V supply to the servo rail input. The FMUK66 is not supplying power to the servo-rail.
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel)
----
FTL stack trace ("~" means nesting-related):
- Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1]
- Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1]
----