How should I power an external device like a "lidar-lite"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How should I power an external device like a "lidar-lite"?

Jump to solution
1,523 Views
nxf58541
NXP Employee
NXP Employee

When I hooked up an external power supply to power sensors on an I2C hub the speaker in the GPS sounds like it blew (all the tones are scratchy) also I don't think Im getting a lock but I have to take it outside to be sure. Any solutions?

0 Kudos
1 Solution
1,457 Views
nxf58541
NXP Employee
NXP Employee

The RDDRONE-FMUK66 schematics, gerbers etc are here: https://www.nxp.com/design/designs/px4-robotic-drone-fmu-rddrone-fmuk66:RDDRONE-FMUK66?&tid=vanRDDRO.... Generally you should not back power the FMU with 5V externally. the signal lines are all 3V, so it could be possible to damage something. But there's nothing obvious as to why the GPS beeper would suffer.

View solution in original post

0 Kudos
1 Reply
1,458 Views
nxf58541
NXP Employee
NXP Employee

The RDDRONE-FMUK66 schematics, gerbers etc are here: https://www.nxp.com/design/designs/px4-robotic-drone-fmu-rddrone-fmuk66:RDDRONE-FMUK66?&tid=vanRDDRO.... Generally you should not back power the FMU with 5V externally. the signal lines are all 3V, so it could be possible to damage something. But there's nothing obvious as to why the GPS beeper would suffer.

0 Kudos