How do I use the Segger JLINK to program my drone FMU? Where do I get the JLINK software?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use the Segger JLINK to program my drone FMU? Where do I get the JLINK software?

Jump to solution
1,633 Views
nxf58541
NXP Employee
NXP Employee

I am trying to program the bootloader onto my FMU but I can't find the Jlink command software on the swegger website? Am I confused or is it part of the "software and documentation pack" in which case there is no jlink command within the pack.

0 Kudos
1 Solution
1,577 Views
nxf58541
NXP Employee
NXP Employee

I think you are asking where to get the JLINK software. Try this: https://nxp.gitbook.io/hovergames/downloads#j-link-software-and-documentation-pack. Then you can run from the command line Jlink.exe. (windows, press the windows button and type cmd first.. to get a command prompt. In the linux VM it is already installed).

View solution in original post

0 Kudos
1 Reply
1,578 Views
nxf58541
NXP Employee
NXP Employee

I think you are asking where to get the JLINK software. Try this: https://nxp.gitbook.io/hovergames/downloads#j-link-software-and-documentation-pack. Then you can run from the command line Jlink.exe. (windows, press the windows button and type cmd first.. to get a command prompt. In the linux VM it is already installed).

0 Kudos