How do I provide power to servos connected to the NXP RDDRONE-FMUK66 PWM output ports?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How do I provide power to servos connected to the NXP RDDRONE-FMUK66 PWM output ports?

跳至解决方案
3,901 次查看
matthiaswilkens
NXP Employee
NXP Employee

I had problems getting servos 5 and 6 working in pass through on the FMU. Something I should have figured out sooner was that power needs to be supplied though the BEC connector to supply the servos in position 5 and 6.

标记 (4)
0 项奖励
回复
1 解答
3,875 次查看
matthiaswilkens
NXP Employee
NXP Employee

I recommend to get an extra BEC. It's indeed the safest option. You don't want to mess with the FMU power module and risk the FMU not receiving enough power at some point. Power should not be pulled from the FMU power module, but instead a 5V BEC should be attached to the power distribution board and the output of the BEC connected to the PWM header marked "BEC". This will supply power to the servos.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,876 次查看
matthiaswilkens
NXP Employee
NXP Employee

I recommend to get an extra BEC. It's indeed the safest option. You don't want to mess with the FMU power module and risk the FMU not receiving enough power at some point. Power should not be pulled from the FMU power module, but instead a 5V BEC should be attached to the power distribution board and the output of the BEC connected to the PWM header marked "BEC". This will supply power to the servos.

0 项奖励
回复
3,852 次查看
BruceHecht
Contributor I

Hi,

Would you have a recommended BEC to use?  Do we connect this from the power distribution board to the PWM controller ?

Thank you!

 

0 项奖励
回复