How can I balance the drone to keep it from drifting? How much drift is expected?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I balance the drone to keep it from drifting? How much drift is expected?

Jump to solution
1,446 Views
nxf58541
NXP Employee
NXP Employee

Does anyone have tips for balancing the drone so that it does not drift when the control sticks are centered? Should I redistribute the weight on the drone, change my controller settings, or do something else (Qground control)?

0 Kudos
1 Solution
1,394 Views
nxf58541
NXP Employee
NXP Employee

Please check that the propellers are all vertical. Note that position hold will hold the position but altitude hold will not. TO actually check the balance you can just hold it using one finger each underneath opposite motors and see if it tilts. Do this on each part of the opposite motors of the X. You can try also balacing on the center line of the drone main body.

View solution in original post

0 Kudos
1 Reply
1,395 Views
nxf58541
NXP Employee
NXP Employee

Please check that the propellers are all vertical. Note that position hold will hold the position but altitude hold will not. TO actually check the balance you can just hold it using one finger each underneath opposite motors and see if it tilts. Do this on each part of the opposite motors of the X. You can try also balacing on the center line of the drone main body.

0 Kudos