Does anyone have tips for balancing the drone so that it does not drift when the control sticks are centered? Should I redistribute the weight on the drone, change my controller settings, or do something else (Qground control)?
解決済! 解決策の投稿を見る。
Please check that the propellers are all vertical. Note that position hold will hold the position but altitude hold will not. TO actually check the balance you can just hold it using one finger each underneath opposite motors and see if it tilts. Do this on each part of the opposite motors of the X. You can try also balacing on the center line of the drone main body.
Please check that the propellers are all vertical. Note that position hold will hold the position but altitude hold will not. TO actually check the balance you can just hold it using one finger each underneath opposite motors and see if it tilts. Do this on each part of the opposite motors of the X. You can try also balacing on the center line of the drone main body.