HoverGames NavQ Google Coral Camera Case on Thingiverse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HoverGames NavQ Google Coral Camera Case on Thingiverse

1,599件の閲覧回数
nxf58541
NXP Employee
NXP Employee

Hi everyone,

The camera on the NavQ as shipped comes protected with heatshrink, and it can be affixed in a variety of locations on the drone with double sided tape or velcro.

For those with access to a 3d printer, i just made a small case with articulated mount and thought i would share it. This aligns with the holes in the drone extension plate that is included with the kit. A screw and standoff kit is included with the NavQ and there are extra pieces that can be used for connecting this to the plate.

You can download the STL files here. I also included STEP and Fusion360 source files if anyone wants to edit anything themselves. (Fusion360 is free for educational use BTW)
https://www.thingiverse.com/thing:4550444

There's a video of it in action included: 

0 返答(返信)