Can I mount the FMU, flight controller, in a different location?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I mount the FMU, flight controller, in a different location?

Jump to solution
2,106 Views
nxf58541
NXP Employee
NXP Employee

From what I understand, mounting the flight controller level with the props is ideal for control (the gyro axes are closer to the vehicle control axes). Would the flight controller handle alright if I offset it a bit by mounting it underneath the quad?

0 Kudos
1 Solution
1,958 Views
nxf58541
NXP Employee
NXP Employee

That should work because the FMU is supposed to be as close to the center of mass of the drone as possible. There are parameters available in PX4 for an IMU position offset within the body frame, but you will probably not need them.
However, you will have to find a solution for the vibration damping when you put the FMU underneath.

View solution in original post

0 Kudos
1 Reply
1,959 Views
nxf58541
NXP Employee
NXP Employee

That should work because the FMU is supposed to be as close to the center of mass of the drone as possible. There are parameters available in PX4 for an IMU position offset within the body frame, but you will probably not need them.
However, you will have to find a solution for the vibration damping when you put the FMU underneath.

0 Kudos