Hello, I am trying to create my own program in C and flash it onto my FMUk66 board. I have been following the gitbook tutorials so far though they don't seem to use MCUXpresso, i thought it should not be a problem. I added my hg_led.c and the cmakelists.txt file in the folder as expressed by the tutorial, but could not find the default.cmake file in the builds/nxp/fmuk66-v3 folder, as it told me to. Unsurprisingly, the example did not show up when i used the MAVlink console in Qgroundcontrol after having flashed the new build. Is has the default.cmake file been moved or is there anything else i might have done wrong?
Here is the tutorial i followed:
https://nxp.gitbook.io/hovergames/developerguide/px4-tutorial-example-code/hg-px4-example-lab-3
The builds/nxp/fmuk66-v3 folder:
And the Firmware/src/examples folder:
Also, i tried making my own default.cmake file in the given directory, and copied the given code, though this also failed.
Thanks in advance.
The error in building https://skytils.com/ likely stems from incorrect toolchain setup or missing dependencies. Double-check board configuration and ensure all SDK paths are correctly set