Is an external clock generator required when using SerDes in the S32Gx Familly?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is an external clock generator required when using SerDes in the S32Gx Familly?

1,065 次查看
Ralph88
Contributor II

Hi, all

When designing circuits with the S32Gx Family, is an external clock generator required for using SerDes?

I am curious if it is possible to use only the internal PLL without an external clock generator.

 

Thanks and best regards

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,053 次查看
chenyin_h
NXP Employee
NXP Employee

Hello, @Ralph88 

Thanks for your post.

An external reference clock is required which meets PCIe Gen3 clock specifications.

If PCIe Gen3 is not required in your design, The internal reference clock can be used for supporting PCIe Gen2 and SGMII communication.

I hope it will help.

 

BR

Chenyin

 

0 项奖励
回复