关于TJA1043电源部分使用问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于TJA1043电源部分使用问题

Jump to solution
273 Views
渊蛟
Contributor I

1.通过查看芯片框图,VCC是驱动器部分(CAN_H、CAN_L)供电电源,VIO是数字部(TX、RX)部分供电电源,那VBAT是哪部分供电呢?规格书中哪部分内容有详细描述这三部分电源的作用?

2.根据应用原理图,通过INH引脚关闭VCC和VIO电源以降低功耗,此时,只有VBAT正常供电,还能保留哪些部分功能呢?

3.是否有TJA1043中文规格书或相关的应用笔记,麻烦给个链接,谢谢!

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
257 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

1. VCC powers the CAN driver circuitry, particularly the CAN_H and CAN_L lines, so it is necessary when the transceiver is actively transmitting and receiving CAN signals.

VIO powers the logic-level interface for the microcontroller, handling digital signals on the TXD, RXD, STB_N, EN and ERR_N.

VBAT is the primary battery power supply. The low power receiver with bus monitor, WAKE circuits and INH are supplied via VBAT. 

You can find additional information in the AH1014 , chapters 7.1 and 6.1.

2. When VCC and VIO are turned off (often achieved by disabling them via the INH pin to reduce power consumption), the transceiver enters Sleep mode, where only VBAT is supplying power.

In this configuration, the TJA1043 retains wake-up functionality, including the ability to monitor for a dedicated wake-up pattern or a digital wake-up signal on the WAKE pin. This  allows the transceiver to transition to Normal mode when a wake-up event is detected, even if VCC and VIO are off.

Other functionality, such as CAN communication or full interfacing with the MCU, will be unavailable until VCC and VIO are re-enabled.

3. As I mentioned before, there is available the AH1014 with necessary information for HW and SW engineers to succesfully implement our 3rd generation HS-CAN transceivers including the TJA1043.

https://www.nxp.com/docs/en/supporting-information/AH1014.pdf

BRs, Tomas

View solution in original post

0 Kudos
Reply
1 Reply
258 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

1. VCC powers the CAN driver circuitry, particularly the CAN_H and CAN_L lines, so it is necessary when the transceiver is actively transmitting and receiving CAN signals.

VIO powers the logic-level interface for the microcontroller, handling digital signals on the TXD, RXD, STB_N, EN and ERR_N.

VBAT is the primary battery power supply. The low power receiver with bus monitor, WAKE circuits and INH are supplied via VBAT. 

You can find additional information in the AH1014 , chapters 7.1 and 6.1.

2. When VCC and VIO are turned off (often achieved by disabling them via the INH pin to reduce power consumption), the transceiver enters Sleep mode, where only VBAT is supplying power.

In this configuration, the TJA1043 retains wake-up functionality, including the ability to monitor for a dedicated wake-up pattern or a digital wake-up signal on the WAKE pin. This  allows the transceiver to transition to Normal mode when a wake-up event is detected, even if VCC and VIO are off.

Other functionality, such as CAN communication or full interfacing with the MCU, will be unavailable until VCC and VIO are re-enabled.

3. As I mentioned before, there is available the AH1014 with necessary information for HW and SW engineers to succesfully implement our 3rd generation HS-CAN transceivers including the TJA1043.

https://www.nxp.com/docs/en/supporting-information/AH1014.pdf

BRs, Tomas

0 Kudos
Reply