please show name of the image when selecting one

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

please show name of the image when selecting one

750件の閲覧回数
PragmaLab
Contributor II

LS,

when I want to select an image for an image button or image object, only the preview of the image is shown to select from, but there is no way to check which image it is since the name is not shown

PragmaLab_0-1681284904253.png

Would it be possible in the next release of GuiGuider to show the name of the image when eg you hoover over the image? Especially with lookalike images (or when experimenting with the same image in a different resolution) it is very hard to know which image is selected

And double-click to select and close the window would be nice too!

Thanks

kind regards,
Rob van Lieshout
PragmaLab

3 返答(返信)

724件の閲覧回数
WenbinYuan
NXP Employee
NXP Employee

Hi Rob,

Thanks for your suggestion about image name when seleted.

Actually in just released version 1.5.1 we have realized this feature, the effect:

image_name_when_selected.png 

Maybe you can try to import your project into new version of GUI Guider to use this feature.

Hope you have a good experience in V1.5.1.

Best Regards,

Wenbin Yuan

0 件の賞賛
返信

729件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @PragmaLab 

 

This feature will be add in next version V1.6.0, thanks!

 

BR

Alice

0 件の賞賛
返信

739件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @PragmaLab 

 

Thanks for your sharing, I think this feature is very useful.  I have taken request to GUI guider team.

Thanks!

 

BR

Alice

0 件の賞賛
返信