lpc5506 keil通过jlink烧写之后黑屏

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc5506 keil通过jlink烧写之后黑屏

ソリューションへジャンプ
1,551件の閲覧回数
papa
Contributor I

我用gui guider 生成keil工程文件之后,通过j-link烧录,提示烧录成功后屏幕并没有显示,这是为什么呢?

0 件の賞賛
1 解決策
1,354件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

Sorry the GUI Guider doesn't support this board so far, recommend you development based on application you mentioned, it includes drivers for your board.

 

BR

Alice

 

元の投稿で解決策を見る

0 件の賞賛
8 返答(返信)
1,511件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

 

你在SDK下找一个GUI guider 的 demo, 烧写进去,查看是否能正常显示。

 

BR

Alice

0 件の賞賛
1,496件の閲覧回数
papa
Contributor I

我烧录官方发来的keil版本的示例程序是正常的,但是gui guider生成的示例程序不能显示,keil和MCUXpresso IDE都不行

0 件の賞賛
1,424件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

Could you please take a screenshot or video about the steps you create project and configuration.

 

BR

Alice

0 件の賞賛
1,407件の閲覧回数
papa
Contributor I

I'm so sorry

For some reason, I couldn't upload the original

3f55dfe3434939902b437ac5df49ac3.jpg微信图片_20230522150651.jpg微信图片_20230522150805.jpg微信图片_20230522150905.jpgf44a6733cc04a15c51e3366da36c094.jpg微信图片_20230522151133.jpg微信图片_20230522151312.jpg微信图片_20230522151315.jpg

 

微信图片_20230522141706.jpg

0 件の賞賛
1,392件の閲覧回数
LiubinGong
NXP Employee
NXP Employee

Hello  

  I'm guessing the root cause is a different panel

  1. We support LPC55s06, and the default panel adafruit-1947(320x240)
  2. Which board in the chosen SDK does it work?  would you please check the panel name and size?

Best Regards 

Liubin

0 件の賞賛
1,381件の閲覧回数
papa
Contributor I

Hello LiubinGong

微信图片_20230522181250.jpg微信图片_20230522181305.jpgThis is what I ported the generated program to the demonstration program.

The initial panel size was adafruit-1947(320x240), but the scale was wrong.

So I'll change the panel size to 480 * 320,as shown in the figure.

0 件の賞賛
1,355件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @papa 

Sorry the GUI Guider doesn't support this board so far, recommend you development based on application you mentioned, it includes drivers for your board.

 

BR

Alice

 

0 件の賞賛
1,350件の閲覧回数
papa
Contributor I
Oh, all right.
0 件の賞賛