deformation of widgets on RT1170 LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

deformation of widgets on RT1170 LCD

ソリューションへジャンプ
2,130件の閲覧回数
ZHOU_XIAO
NXP Employee
NXP Employee

Hello all.

I am using the Gui Guider 1.4.0 to create easy sample for RT1170 promotion demo.

The widgets of switch and slides shows well in the simulators (C language)

ZHOU_XIAO_0-1663650053619.png

 

 

However after I write and run the project into target RT1170 with LCD(RK055HDMIPI4M) ,the widgets shows changed and deformation as following pictures

ZHOU_XIAO_1-1663650138797.png

 

By the way I just add these switch and slides widgets by default without any modification.

 

 

Best regards

ZHOU

0 件の賞賛
返信
1 解決策
2,096件の閲覧回数
Haibao
NXP Employee
NXP Employee

Hi @ZHOU_XIAO 

There is one workaround for this, you can disable the VGlite under LvConf of IDE setting.

BRs,

Haibao

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,108件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @ZHOU_XIAO ,

I just see this bug is fixed in new version, GUI Guider v1.4.1 RC2. It is in field trial.

 

Regards,

Jing

 

Regards,

Jing

0 件の賞賛
返信
2,097件の閲覧回数
Haibao
NXP Employee
NXP Employee

Hi @ZHOU_XIAO 

There is one workaround for this, you can disable the VGlite under LvConf of IDE setting.

BRs,

Haibao

0 件の賞賛
返信