create new project , show "download is failed please check your network"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

create new project , show "download is failed please check your network"

3,024件の閲覧回数
hubo0831
Contributor I

first use GUI Guider 1.8.0,  select sim and empty ui, when create new project , show "download is failed please check your network", but network is good, how to solve?

0 件の賞賛
返信
8 返答(返信)

2,057件の閲覧回数
sjg
Contributor I

上面的问题解决了吗?我也遇到这个问题,运行v1.61 ,v1.70版本正常,v1.80的才有这问题

0 件の賞賛
返信

2,050件の閲覧回数
sjg
Contributor I
试了多个版本,发现从v1.72开始都有这个问题,且打开后软件的菜单语言是英文的(安装时已选择为中文)
0 件の賞賛
返信

2,057件の閲覧回数
sjg
Contributor I
已卸载重新安装了两次,结果还是一样无法创建新的空白工程,提示下载失败
0 件の賞賛
返信

2,711件の閲覧回数
hubo0831
Contributor I

can you tell me, what cause this error, reinstall is invalid

0 件の賞賛
返信

2,983件の閲覧回数
hubo0831
Contributor I

I alse install V1.7.2, it has same error

0 件の賞賛
返信

2,823件の閲覧回数
Alphabert_Liu
NXP Employee
NXP Employee

Dear @hubo0831 ,

I'm sorry, but I don't reproduce the problem you mentioned. If the error persists, you can try to uninstall the Gui Guider completely and reinstall it again.

Best Regard

Liu

0 件の賞賛
返信

2,990件の閲覧回数
hubo0831
Contributor I

creage project again, it also is same error,see screenshots 

微信图片_20240731153545.png微信图片_20240731153642.png

0 件の賞賛
返信

2,995件の閲覧回数
WenbinYuan
NXP Employee
NXP Employee

Hello @hubo0831,

 

Please try the following steps to resolve the issue:

  1. Restart the GUI Guider and reset your network connection, then attempt to create the project again.
  2. Download the offline template and configure it according to the user guide then trying to create the project again.
  3. Try creating the project using an earlier version, such as V1.7.2, to check the network connectivity.

If the problem persists, please provide us with screenshots of the error messages, and we will further analyze the cause of the issue.

Thank you for your patience and cooperation.

Best regards,

Wenbin

0 件の賞賛
返信