I cannot open the software

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I cannot open the software

跳至解决方案
616 次查看
Wisam
Contributor II

Unhandled Promise Rejection
Error: ERR_FAILED (-2) loading 'file:///D:/NXP/GUI-Guider-1.9.1-GA/resources/welcome.html'
at rejectAndCleanup (node:electron/js2c/browser_init:165:7510)
at EventEmitter.stopLoadingListener (node:electron/js2c/browser_init:165:7885)
at EventEmitter.emit (node:events:539:35)

0 项奖励
回复
1 解答
544 次查看
Wisam
Contributor II

Thank you for your reply. After I changed the installation path to the C drive, the error no longer appeared.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
552 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @Wisam 

That error means the GUI Guider app  is failing to load its built-in HTML resources.
Specifically, it can’t open:

file:///D:/NXP/GUI-Guider-1.9.1-GA/resources/welcome.html

Did you install GUI Guider to C:\ or move it manually to D:\?

BR

Harry

0 项奖励
回复
545 次查看
Wisam
Contributor II

Thank you for your reply. After I changed the installation path to the C drive, the error no longer appeared.

0 项奖励
回复
613 次查看
Wisam
Contributor II

The version I downloaded is 1.9.1 and runs on Windows 11.

0 项奖励
回复