GuiGuider 1.5.0 generated projects won't build in MCUXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GuiGuider 1.5.0 generated projects won't build in MCUXpresso

Jump to solution
1,738 Views
PragmaLab
Contributor II

Hello all,

I updated to GuiGuider 1.5.0 some weeks ago and was happy to see that NXP kindly fixed the issues I wrote about earlier in this forum. Thanks for that.

Please note that ' out of the box'  generated MCUXpresso won't build in MCUXpresso due to missing lib-path includes:

  • cannot find -lopenh264
  • cannot find -lrlottie

To fix this, you need to have:

-L"<path to your project folder>\lib\x86"

in your buildsettings for the linker. Adding this path (for me) only works by adding the path using the 'Filesystem direcory' method. The 'Workspace'  method won't work (lib-subfolders are invisible in the project settings).

Breaking with the MCUXpresso project path and having to include libs from a \x86 (?) folder doesn't feel right. All for the sake of linking to H264 decoders and animation stuff which I don't even use in my GuiGuider project?

I suppose either this library search path needs to get included by default in the projects settings, or some option in GuiGuider should be introduced to disable the need for these 2 new features?

Furthermore the 1.5.0 manual seems missing?

kind regards

Rob

0 Kudos
Reply
1 Solution
1,629 Views
LiubinGong
NXP Employee
NXP Employee

Hello Pragmalab

  Thanks for your feedback, We know the reason for this problem, and it will be resolved in the next release. and workaround:  Create a new project based on your local project, which will work fine.

Best Regards

Liubin 

View solution in original post

0 Kudos
Reply
5 Replies
1,708 Views
LiubinGong
NXP Employee
NXP Employee

Hello Pragmalab

   Thanks for your finding. In order to better fix the issue. Can you provide the following information clearly? 

  • host system environment
  • old project or newly created 
  • which platform

Thanks 

Liubin

0 Kudos
Reply
1,640 Views
PragmaLab
Contributor II

Sorry I wasn't clear on about the setup:

  • my GUI development takes place on a Windows 11 Pro (version22H2) PC
  • the project reported in the bug is an old (existing) project that was migrated to GuiGuider 1.5.0
  • the platform is an IMXRT1052 EVK board (using a 480 x 272 display)
  • I'm using MCUXpresso 11.6.1 with SDK 2.13.0

MCUXpresso does tricky  things when showing paths and files. It never represents the file-tree as being present on disc. In stead  it will present its  workspace file tree. I guess that makes that I can't add the lib path by choosing the Workspace option. 

Do we realy need the libs in the \x86 folder to build the (crossplatform) project? Aren't these libs meant for the simulator ?

 

kind regards,

Rob

 

0 Kudos
Reply
1,721 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Thanks again to find that's bugs, we are checking it

0 Kudos
Reply
1,639 Views
PragmaLab
Contributor II

...forgot to mention. The 1.5.0 manual is available from within the IDE (Help -> User Guide) but on the GuiGuider NXP info page (https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER) only the 1.4.0 manual is available for download... (while the page announces the 1.5.0 version)

0 Kudos
Reply
1,630 Views
LiubinGong
NXP Employee
NXP Employee

Hello Pragmalab

  Thanks for your feedback, We know the reason for this problem, and it will be resolved in the next release. and workaround:  Create a new project based on your local project, which will work fine.

Best Regards

Liubin 

0 Kudos
Reply