GUI Guider examples Horizontal vs Vertical

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GUI Guider examples Horizontal vs Vertical

跳至解决方案
173 次查看
SolitoFrancesco
Contributor I

Hello

I noticed that if I open an example project for MIMXRT1170-EVK, the default settings seem to be for vertical display, but then all the pictures "are stretched". If instead I modify the Panel Type in a "custom" way (so I put the same panel name RK055MHD091) using width=1280 and height=720, the pictures are represented correctly as expected.

I would like to have a confirmation that this is the normal behavior or not (because to be honest I expect to get the example already working correctly in horizontal way, so my doubt is that I'm making something wrong on another setting of GUI Guider or in a HW setting of the evaluation board).

Thnak you and kind regards,

Francesco

0 项奖励
回复
1 解答
143 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @SolitoFrancesco,

Yes, this would be the method to use on versions of GUI Guider that don't have the option of 1280x720 natively.

That said, I would like to add a recommendation to make sure you are using the latest version of GUI Guider (v1.10.0).

BR,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
144 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @SolitoFrancesco,

Yes, this would be the method to use on versions of GUI Guider that don't have the option of 1280x720 natively.

That said, I would like to add a recommendation to make sure you are using the latest version of GUI Guider (v1.10.0).

BR,
Edwin.

0 项奖励
回复
133 次查看
SolitoFrancesco
Contributor I

Thank you. To be honest it seems to be that also in GUI Guider 1.10.0 there isn't a horizontal option 720x1280. Anyway it's not a problem. Thanks for confirmation that I'm doing the correct thing.

Kind regards,

Francesco  

0 项奖励
回复