GUI Guider 1.5.0 模拟时钟指向方向不对以及图片出现锯齿的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GUI Guider 1.5.0 模拟时钟指向方向不对以及图片出现锯齿的问题

1,782 Views
YoungWind
Contributor III

你好!

我在使用模拟时钟控件是发现了两个问题:

1.模拟时钟时针、分针、秒针使用图片时,不管怎么调整都无法指向真正的位置

YoungWind_0-1676904705831.png

YoungWind_5-1676905338565.png

 

2.转向某一个角度时,图片锯齿特别严重

A:这个角度时,图片没有锯齿

YoungWind_1-1676904998167.png

B:这个角度时,图片有锯齿

YoungWind_2-1676905061458.pngYoungWind_3-1676905106858.png

YoungWind_4-1676905147198.png

 

 

 

坚持做自己喜欢的事
0 Kudos
7 Replies

1,759 Views
zhenhualuo
NXP Employee
NXP Employee

Hi @YoungWind,

Can you please try to change the value of "rotation center" attribute and check if image needle can point to right position? If the issue persists, please share your needle image with us, then we can try to reproduce the issue and find out the solution..

Best Regards,

Zhenhua

0 Kudos

1,754 Views
YoungWind
Contributor III

你好!我尝试了通过调节旋转中心来指向我想要指向的位置,但是还是失败了。

以下是我使用到的图片素材

watch_sec_gentle.png

坚持做自己喜欢的事
0 Kudos

1,737 Views
zhenhualuo
NXP Employee
NXP Employee

Hi @YoungWind,

Thanks for sharing the image, I have tried the image needle, can you please take a look the value of rotate center setting and check if this is the expected effect? 

1.png

2.png

Best Regards,

Zhenhua

1,727 Views
YoungWind
Contributor III

 谢谢你的回复,但是我按照您的属性配置后,发现还是无法实现像您图片中的效果

YoungWind_0-1677073706428.png

但是我发现一个细节,您导入的图片指针方向是横着的,我导入的是竖着的,请问图片方向您是经过转换过的吗?

 

坚持做自己喜欢的事
0 Kudos

1,700 Views
zhenhualuo
NXP Employee
NXP Employee

Hi @YoungWind,

Yes, I rotate the image to the horizontal direction, please see attached image.

watch_sec_gentle.png

Best Regards,

Zhenhua

0 Kudos

1,695 Views
YoungWind
Contributor III

好的,谢谢!我实现了。

要是背景和中心的圆点能自定义更改那几太好了

坚持做自己喜欢的事
0 Kudos

1,662 Views
zhenhualuo
NXP Employee
NXP Employee

Hi @YoungWind,

Great to see that you implemented the expected effect.

It is a good suggestion to support custom background and center point, we will add the function in roadmap and support in future release. As a workaround, you may use image widget to set the background picture and center point.

Best Regards,

Zhenhua

0 Kudos