Bug in font generation in V18.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug in font generation in V18.0?

605 Views
TsuyoshiSugiyama
Contributor II

When generating fonts in V18.0, the font height changes.
For example, when creating a font with a height of 24px, the height has changed to 29px.
This makes it impossible to use the UI I have created so far.
Is this a bug? Even if it is a specification, it is still a problem.

TsuyoshiSugiyama_0-1723188652647.png

 

0 Kudos
Reply
2 Replies

588 Views
Alphabert_Liu
NXP Employee
NXP Employee

Dear @TsuyoshiSugiyama ,

29 here refers to the line height, which refers to the height of a line of text, including the height of the characters themselves and the line spacing.If you want, you can reduce the font line spacing.

Best Regard

Liu

0 Kudos
Reply

464 Views
TsuyoshiSugiyama
Contributor II

Thank you for your answer.
How can I reduce the line spacing of the font?
We designed the UI at 24px, so there are problems if that is changed.

Best Regard

0 Kudos
Reply