无法登入GUI GUIDET -1.9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

无法登入GUI GUIDET -1.9

1,139件の閲覧回数
zls66336
Contributor I

打开Gui Guider-1.9会弹出一个登入界面,使用我注册的账户提示校验失败。

0 件の賞賛
返信
8 返答(返信)

1,061件の閲覧回数
sgf201
Contributor I

确实解决了

0 件の賞賛
返信

1,067件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @zls66336 @jiadandan @sgf201 @mark2 

We have resolved the login issue. You can try logging in.

Sorry for any inconvenience caused.

BR

Harry

1,043件の閲覧回数
jiadandan
Contributor II
已经可以登陆了,赞赞!
0 件の賞賛
返信

1,080件の閲覧回数
jiadandan
Contributor II

遇到了同样的问题;

タグ(1)
0 件の賞賛
返信

1,095件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zls66336@sgf201 and @mark2 

Currently the GUI Guider login is experiencing issues, as you mention. The GUI Guider team is aware of this issue and actively working on it to resolve it as soon as possible. Please be patient while the problem is resolved.

I apologize for the inconvenience.

BR,
Edwin.

0 件の賞賛
返信

1,115件の閲覧回数
sgf201
Contributor I

我也有同样的问题

0 件の賞賛
返信

1,135件の閲覧回数
mark2
Contributor III
我也有同样的问题。

 

0 件の賞賛
返信

1,116件の閲覧回数
sgf201
Contributor I
 
0 件の賞賛
返信