Release Announcement - GUI Guider v1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Release Announcement - GUI Guider v1.1

Release Announcement - GUI Guider v1.1

The latest version of GUI Guider was recently released by NXP. If you are unfamiliar with GUI Guider it is a graphical development tool for creating UIs on supported NXP microcontrollers. The tool allows you to create a UI, test the UI along with various levels of events all within a simulation environment, and then deploy the UI application directly to the NXP development board or generate the code for use in MCUXpresso IDE. GUI Guider is designed specifically for use with LVGL, an open-source graphics library, that is available within the MCUXpresso SDK.

 

This release of GUI Guider features:

  • New Development Tool capabilities
    • Menu shortcut and keyboard control
    • New states: FOCUSED, EDITED, DISABLED
    • Frame rate customization
    • Screen transition configuration
    • Parent / children widgets
    • Callback function setting for animation image
    • VGLite enablement
    • Header path auto-config

  • New or improved Widgets
    • BMP and SVG assets
    • 3D animation for PNG

  • HW Acceleration capabilities
    • Initial support for VGLite on RT1170 and RT595

  • New Device Target Supported

Attachments
100% helpful (1/1)
Version history
Last update:
‎05-27-2021 09:48 AM
Updated by: