freemaster

取消
显示结果 
搜索替代 
您的意思是: 

freemaster

560 次查看
song123
Contributor I

Why is the "pig in module" drop-down menu blank?

song123_1-1663556764305.jpeg

 

0 项奖励
3 回复数

531 次查看
MichalH
NXP Employee
NXP Employee

Hello,

this seems as a problem of installation - it must be run with administrator rights.

You can easily fix it by running the C:\NXP\FreeMASTER 3.2\FreeMASTER\register.bat as an administrator (select the file in Windows Explorer, pull a context menu and select "Run as administrator").

If this does not help, re-start the installer also with administrator rights.

Regards,
Michal

 

MichalH_1-1663741585660.png

 

 

518 次查看
song123
Contributor I

Thanks, this is very useful

0 项奖励

482 次查看
MichalH
NXP Employee
NXP Employee

Thanks. If this solves your issue, please mark this and the other question as resolved.

Regards,
Michal