freemaster无法安装

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freemaster无法安装

2,017 Views
1111
Contributor I

freemaster无法安装错误提示

错误提示信息:

One or more newer versions of the product are already installed. An upgrade is not applicale

C:\INXPIFreeMASTER 3.1

0 Kudos
5 Replies

2,003 Views
iulian_stan
NXP Employee
NXP Employee

Hi @1111,

Could you check this thread.

Hope it helps,
Iulian

0 Kudos

1,998 Views
1111
Contributor I
0 Kudos

2,000 Views
1111
Contributor I
安装好之后为什么不用输入激活码?不用输入激活码可以用吗?
0 Kudos

1,994 Views
iulian_stan
NXP Employee
NXP Employee

The activation code is required only for FreeMASTER Lite component. You can use main FreeMASTER tool without activation code - just unselect "FreeMASTER Lite" option during installation.

Note: FreeMASTER Lite license is free of charge, you just need to have an account on NXP web site.

0 Kudos

1,991 Views
1111
Contributor I

在安装过程中取消或者勾选 " Free MaSTER Lite "选项都不需要激活码

0 Kudos