PCANBasic.dll not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCANBasic.dll not found

跳至解决方案
581 次查看
sobo
Contributor III

Hello,

I try to use FreeMAster on CAN with a PEAK can.
I installed Freemaster 3.2

I copied the PCANBasic.dll from that i downloaded from PEAK can PCAN, I copied the x86 version.
I rebooted the PC.

but I've got this error :

sobo_0-1756302119451.png

what's my next step ?

 

Sophie

FREEMASTER 




标记 (2)
0 项奖励
回复
1 解答
551 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,

I tried to test on a clean Windows 11/64bit machine: Before PCAN drivers were installed, the message was the same as yours. After installing the PCAN Win11 drivers from this link, the FreeMASTER shows the PCANBasic.dll is loaded successfully.

For now, this is the only test I can do. I will be able to try more with a PCAN device during next week. I will inform you then.

Please try to reinstall the PCAN drivers and reboot. Also check the DLLs:

  • The C:\Windows\SYSTEM32\PCANBasic.dll is the x64 version which the FreeMASTER attempts to load, but the system automatically uses the x86 version instead.
  • The x86 version must exist at: c:\Windows\SysWOW64\PCANBasic.dll 

In my case, the properties of c:\Windows\SysWOW64\PCANBasic.dll  show:

MichalH_0-1756369754310.png

 

Regards,
Michal

在原帖中查看解决方案

0 项奖励
回复
2 回复数
525 次查看
sobo
Contributor III

Thank you Michal.

Now Freemaster can finf the DLL now

 

Sophie

0 项奖励
回复
552 次查看
MichalH
NXP Apps Support
NXP Apps Support

Hello,

I tried to test on a clean Windows 11/64bit machine: Before PCAN drivers were installed, the message was the same as yours. After installing the PCAN Win11 drivers from this link, the FreeMASTER shows the PCANBasic.dll is loaded successfully.

For now, this is the only test I can do. I will be able to try more with a PCAN device during next week. I will inform you then.

Please try to reinstall the PCAN drivers and reboot. Also check the DLLs:

  • The C:\Windows\SYSTEM32\PCANBasic.dll is the x64 version which the FreeMASTER attempts to load, but the system automatically uses the x86 version instead.
  • The x86 version must exist at: c:\Windows\SysWOW64\PCANBasic.dll 

In my case, the properties of c:\Windows\SysWOW64\PCANBasic.dll  show:

MichalH_0-1756369754310.png

 

Regards,
Michal

0 项奖励
回复