Hello. Tomas Fedor
The results of your inquiry are as follows.
1) Are you using OPENSDA interface for flashing the microcontroller or are you using external debugger?
A fault occurred when I ran the project, so I wanted to find the cause. So I tried running FreeMASTER using OPENSDA, and then tried running FreeMASTER using MULTILINK. As a result, faults occurred in both cases.
2) When you disconnect the motor does overcurrent fault appear?
I don't know what indicates an overcurrent fault in FreeMASTER. So I attached the picture below.
- motor connect (Phase A~C wire connected) : Value of overcurrent related variable - 1
- motor disconnect (Phase A~C wire disconnected) : 1 (Same result as above)
motor connect (Phase A~C wire connected)

motor disconnect (Phase A~C wire connected)

3) Could you measure the voltages on DEVKIT-MOTORGD J9, J10, J11 pin 2 (with jumper setting for PMSM 1-2)
I measured the voltage between pin2 of J9, J10, J11 and gnd. Why is this voltage needed?
J9 : 2.491V
J10 : 2.507V
J11 : 2.512V
4) Could you measure the voltages on DEVKIT-MOTORGD test point TP1 and J3 PIN3.
A short occurred while measuring the voltage between TP1 and J3 pin3. I applied power to the DEVKIT-MOTORGD board, but it does not work. So I couldn't measure the voltage... Why is this voltage needed?