Hello:
Last month,I installed the FreeMASTER ,and it could connect my board FRDMKE15Z. Yesterday I upgraded the newer version, but it could't connect the board.thus,I delected all the floders about FreeMASTER3.0 to uninstall it.after that,I try many times to re-install ,but every time it shows "one or more newer versions of the product are already installed.An upgrade is not applicable."what should i do ?
I'm looking forward for your reply.
Solved! Go to Solution.
 pavelrech
		
			pavelrech
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
in my case the FreeMASTER can run with no issue. Please check following steps:
Thanks
Pavel
Hello,
I'm having the same problem as you.Did you solve this problem?
 
					
				
		
 MichalH
		
			MichalH
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Dear Yonghui Wang,
so the installation issue is now resolved. How about the communication with the FRDM-KE15z board? Is it working now?
You wrote above that you use the USB to connect FreeMASTER but I need more information. There are two modes in which you can use the physical USB connection with KE15:
Which one do you use and what error do you get? Can you send any screenshot showing the error?
Thanks,
Michal
Hi Michal,
Before the newer FreeMASTER to connect the board, I meet the other problem that the demo project "frdme15z_touch_sensing" and "frdm15z_frmstr_example_usart" can't be build successfully,it has three errors.But the other project can be builded ande debugged successfully,such as "frdmke15z_tsi_v5_selfmode".It seems that if the project about FreeMASTER can't be build.
The console shows:
09:35:02 **** Incremental Build of configuration Debug for project frdmke15z_touch_sensing ****
make -r -j4 all 
Building target: frdmke15z_touch_sensing.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -Xlinker -Map="frdmke15z_touch_sensing.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m0plus -mthumb -T frdmke15z_touch_sensing_Debug.ld -o "frdmke15z_touch_sensing.axf" ./utilities/fsl_assert.o ./utilities/fsl_debug_console.o ./utilities/fsl_str.o ./touch_sensing/source/system/nt_system.o ./touch_sensing/source/system/nt_system_frmstr.o ./touch_sensing/source/system/nt_system_mem.o ./touch_sensing/source/safety/nt_safety.o ./touch_sensing/source/safety/nt_safety_crc.o ./touch_sensing/source/safety/nt_safety_gpio.o ./touch_sensing/source/modules/nt_module_gpio.o ./touch_sensing/source/modules/nt_module_gpioint.o ./touch_sensing/source/modules/nt_module_tsi.o ./touch_sensing/source/modules/nt_modules.o ./touch_sensing/source/keydetectors/nt_keydetector_afid.o ./touch_sensing/source/keydetectors/nt_keydetector_safa.o ./touch_sensing/source/keydetectors/nt_keydetector_usafa.o ./touch_sensing/source/filters/nt_filters.o ./touch_sensing/source/electrodes/nt_electrodes.o ./touch_sensing/source/drivers/tsi/nt_drv_tsi_common.o ./touch_sensing/source/drivers/tsi/nt_drv_tsi_driver.o ./touch_sensing/source/drivers/tsi/nt_drv_tsi_v5_driver_specific.o ./touch_sensing/source/controls/nt_control_arotary.o ./touch_sensing/source/controls/nt_control_aslider.o ./touch_sensing/source/controls/nt_control_keypad.o ./touch_sensing/source/controls/nt_control_matrix.o ./touch_sensing/source/controls/nt_control_proxi.o ./touch_sensing/source/controls/nt_control_rotary.o ./touch_sensing/source/controls/nt_control_slider.o ./touch_sensing/source/controls/nt_controls.o ./touch_sensing/source/nt.o ./startup/startup_mke15z7.o ./source/main.o ./source/mtb.o ./source/nt_setup.o ./source/semihost_hardfault.o ./freemaster/drivers/mcuxsdk/serial/freemaster_serial_lpsci.o ./freemaster/drivers/mcuxsdk/serial/freemaster_serial_lpuart.o ./freemaster/drivers/mcuxsdk/serial/freemaster_serial_miniusart.o ./freemaster/drivers/mcuxsdk/serial/freemaster_serial_uart.o ./freemaster/drivers/mcuxsdk/serial/freemaster_serial_usart.o ./freemaster/drivers/mcuxsdk/serial/freemaster_serial_usb.o ./freemaster/drivers/mcuxsdk/can/freemaster_flexcan.o ./freemaster/drivers/mcuxsdk/can/freemaster_mcan.o ./freemaster/drivers/mcuxsdk/can/freemaster_mscan.o ./freemaster/freemaster_appcmd.o ./freemaster/freemaster_can.o ./freemaster/freemaster_pdbdm.o ./freemaster/freemaster_pipes.o ./freemaster/freemaster_protocol.o ./freemaster/freemaster_rec.o ./freemaster/freemaster_scope.o ./freemaster/freemaster_serial.o ./freemaster/freemaster_sha.o ./freemaster/freemaster_tsa.o ./freemaster/freemaster_utils.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_crc.o ./drivers/fsl_ftm.o ./drivers/fsl_gpio.o ./drivers/fsl_lpit.o ./drivers/fsl_lpuart.o ./drivers/fsl_smc.o ./drivers/fsl_tsi_v5.o ./device/system_MKE15Z7.o ./component/uart/lpuart_adapter.o ./component/serial_manager/serial_manager.o ./component/serial_manager/serial_port_uart.o ./component/lists/generic_list.o ./board/board.o ./board/clock_config.o ./board/pin_mux.o
Memory region Used Size Region Size %age Used
 PROGRAM_FLASH: 77392 B 256 KB 29.52%
 SRAM: 7664 B 32 KB 23.39%
d:/nxp/mcuxpressoide_11.2.0_4120/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.2.0.202001021529/tools/bin/../lib/gcc/arm-none-eabi/9.2.1/../../../../arm-none-eabi/bin/ld.exe: ./freemaster/freemaster_protocol.o: in function `FMSTR_ProtocolDecoder':
C:\Users\Axent\Documents\MCUXpressoIDE_11.2.0_4120\workspace\frdmke15z_touch_sensing\Debug/../freemaster/freemaster_protocol.c:257: undefined reference to `FMSTR_UresControl'
collect2.exe: error: ld returned 1 exit status
 FLEX_RAM: 0 GB 2 KB 0.00%
make: *** [makefile:52: frdmke15z_touch_sensing.axf] Error 1
"make -r -j4 all" terminated with exit code 2. Build might be incomplete.
09:35:07 Build Failed. 3 errors, 0 warnings. (took 5s.245ms)
Thanks,
Yonghui Wang
 pavelrech
		
			pavelrech
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
I cannot simulate your issue. I download SDK 2.8.0 pack with Touch middleware, imported both projects: frdme15z_touch_sensing" and "frdm15z_frmstr_example_usart" and successfully build both examples without any errors. The file freemaster_ures.c was added in both examples after import to MCUX IDE. I would try to create new workspace and import the project you want to use again.
Thanks,
Pavel
Hello,
I tried to create new workspace in new path and import the project ,it also had the error.besides,I installed the SDK 2.7.0,it also has the problem.
Thansk,
Yonghui
 pavelrech
		
			pavelrech
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
ok I will try to investigate your error case, could you provide SDK_package version 2.8.0 you are using and your MCUX IDE version ?
Hello,
MCUX IDE version are 11.0.1_2563 and 11.2.0_4120. The SDK_package version 2.8.0 was downloaded from https://mcuxpresso.nxp.com/download/eec911f9b650b9aecd0fe06f4b218bbe
 pavelrech
		
			pavelrech
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
Firstly I tried to import your SDK 2.8.0 pack into old MCUX IDE 11.0.1_2563 this should not be working and really is not working because old MCUX IDE does not support the new SDK pack 2.8.0 this is expected behavior.
Secondly I tried to import both projects: touch_sensing" and "frmstr_example_uart" from your SDK package into new MCUX IDE 11.2.0_4120, the import and build passed without any error. I checked that FreeMASTER sources are located in your pack you shared in the Wed_Jul_22_12_25_23_2020-windows-mcuxpresso-FRDM-KE15Z.zip\middleware\freemaster\src\ path - this is correct. But you wrote in previous message that you do not see these files in SDK package, how it is possible ?
Did you share mi the same SDK pack you are using ?
If there are not FreeMASTER sources in the SDK pack the sources will not be in the project causing the build issue.
Thank you.
Pavel
Hello,
To the version 11.0.1_2563, I used the SDK 2.7.0,and to the version 11.2.0_4120,I used the SDK 2.8.0. I just checked the SDK zip, found the file freemaster_ures.c,but the unzip folder has not the file ,so amazing.I copy the file into the the unzip folder,now it can build successfully.
After that,I downloaded the program,and disconnected the MCUX IDE11.2.0_4120. But FreeMASTER also can't connect the board,the following picture shows the error (the FreeMASTER project "NXPTouchkez15.pmpx" imported from SDK_2.8.0_FRDM-KE15Z\middleware\touch\freemaster)
Thanks.
 pavelrech
		
			pavelrech
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
in my case the FreeMASTER can run with no issue. Please check following steps:
Thanks
Pavel
Hello,
Now, the FreeMASTER can connect to the board,thank you for your help.
 
					
				
		
 MichalH
		
			MichalH
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
I'm sorry I don't know the Touch solution for KE15, but from the error it seems that the file freemaster_ures.c is not added to project. Do you have the file in the Touch demo installation? If yes, please add it to project. If not, let me know.
Thanks,
Michal
Dear Michal,
      I have been built successfully.I downloaded the program,and disconnected the MCUX IDE11.2.0_4120. But FreeMASTER also can't connect the board,the following picture  shows the error (the FreeMASTER project "NXPTouchkez15.pmpx"  imported from SDK_2.8.0_FRDM-KE15Z\middleware\touch\freemaster).
Thanks.
Hello,
As you said , the project don't have the file freemaster_ures.c .But I can't find the file in the SDK_2.8.0_FRDM-KE15Z\middleware\freemaster\src,and I didn't find the file on my PC.
Thanks,
yonghui
 iulian_stan
		
			iulian_stan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi 1141886202@qq.com,
Regarding the installation issue - it is possible that there are some remaining resources not cleared after the uninstall process.
To confirm this you'll need to check the following file .com.zerog.registry.xml (it should be stored in C:\Program Files (x86)\Zero G Registry). This file contains a xml formated list of products installed using the same packager as FreeMASTER installer. In case it contains only FreeMASTER <product> - just delete the file. Otherwise remove this entry from the <products> list (in this case make a backup copy of the file just in case). After this try launching FreeMASTER installer.
Hope this helps,
Iulian
Hi Iulian,
The problem has been resolved, thank you very much.
 
					
				
		
 MichalH
		
			MichalH
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello,
I don't think that your connection issue with KE15Z was caused by updating to the latest FreeMASTER 3.0. The latest version (3.0.3) is almost the same as the earlier 3.0.x versions, at least in terms of physical communication.
If possible, please install (repair) the latest 3.0.3 and try again. I will assist you to get the communication working. And if we have really broken something in the communication, it will at least help us to find the issue and fix it.
So, if you'd try the 3.0.3, what communication error do you get? What communication type do you use (Serial, JTAG, ..) And can you share your project?
You can reach out to me directly in case you do not want to share the project here in public.
Thanks,
Michal
Michal:
Hello !
Thank you for your reply on the NXP community about my question "how to re-install FreeMASTER".
I installed the newest version 3.0.3.6,it also showed "one or more newer versions of the product are already installed.An upgrade is not applicable."Beside, I tried to uninstall MCUXpresso and delete all folder about NXP ,after that I try again install the newest version 3.0.3.6,the question still exist.
The project what i used is frdmke15z_tsi_v5_selfmodd which imported from SDK example(SDK_2.x_FRDM-KE15z 2.8.0).And I used the USB to connect the Board,now Ican Debug it.
    Does it will cause the problem by deleting the folder about FreeMASTER instead of  using the normal way to uninstall it ?or beause of the Software Activation Code?