Getting started with S32K146EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Getting started with S32K146EVB

跳至解决方案
1,464 次查看
Meneglier
Contributor I

Hello, I have some difficulty with the board S32K146EVB when I try to use the demo application FreeMASTER like the quick start guide :

The board is well connected with port com3 : 115000 bd

The JumpStart project will be automaticaly downloaded from www.nxp.com Once the FreeMASTER application detects the web address stored as an TSA active content in the flash memory of the S32K146 MCU, the download of the FreeMASTER project from www.nxp.com will be initiated.

A error message appear :

Meneglier_0-1678357684175.png

 

0 项奖励
回复
1 解答
1,364 次查看
iulian_stan
NXP Employee
NXP Employee

The URL issue was fixed, updated firmware can be downloaded from S32K146 product page.

FreeMASTER (PC) project is also available on the same page for offline mode.

Capture.PNG

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,453 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @Meneglier,

Please find attached FreeMASTER project.
Open it directly in FreeMASTER tool, then connect to your board. 

Kind regards,
Iulian

0 项奖励
回复
1,365 次查看
iulian_stan
NXP Employee
NXP Employee

The URL issue was fixed, updated firmware can be downloaded from S32K146 product page.

FreeMASTER (PC) project is also available on the same page for offline mode.

Capture.PNG

 

0 项奖励
回复