FreeMaster3.0 Installation failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FreeMaster3.0 Installation failed

跳至解决方案
2,031 次查看
xgy_upc
Contributor III

The error shown in Figure 1 occurred when I installed Freemaster3.0.How can I solve this problem?

figure1.jpg

0 项奖励
回复
1 解答
1,978 次查看
iulian_stan
NXP Employee
NXP Employee

Hi,

Before troubleshooting this issue, please note that activation is required only by FreeMASTER Lite component, in case you are using FreeMASTER (main desktop application) just disable Lite feature in component selection step during installation process.

pastedImage_6.png

Troubleshooting:

  • Make sure you have admin rights on your machine, as there may be some settings blocking the communication between your computer and the licensing server (ex: a firewall).
  • In case you cannot run the installer with admin privileges you can try an offline activation. The process is similar to the one described in this post HOWTO: Activate S32 Design Studio. Note that it is not excluded that you may run into into other issues due to limited access rights.

Hope this helps,

Iulian

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,979 次查看
iulian_stan
NXP Employee
NXP Employee

Hi,

Before troubleshooting this issue, please note that activation is required only by FreeMASTER Lite component, in case you are using FreeMASTER (main desktop application) just disable Lite feature in component selection step during installation process.

pastedImage_6.png

Troubleshooting:

  • Make sure you have admin rights on your machine, as there may be some settings blocking the communication between your computer and the licensing server (ex: a firewall).
  • In case you cannot run the installer with admin privileges you can try an offline activation. The process is similar to the one described in this post HOWTO: Activate S32 Design Studio. Note that it is not excluded that you may run into into other issues due to limited access rights.

Hope this helps,

Iulian

0 项奖励
回复