FreeMASTER graph color changes back to black

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMASTER graph color changes back to black

ソリューションへジャンプ
2,561件の閲覧回数
arun07
Contributor III

Hi All,

I am using FreeMASTER with a custom board based on MKE15Z micro-controller for tuning touch parameters.

Everything is working well, but I am facing some challenges with FreeMASTER regarding the color of variables plotted on the graph.

Whenever I want to see an electrode scope (graphical view with predicted, baseline, noise floor, etc. graphically), then by default color shown is black for all the lines, and after changing it works fine but if I select some other electrode and come back to the electrode for which I have adjusted the colors, it is again shown in black color.

Example: I started viewing Electrode 1, the plot lines are shown in black color.

FreeMASTER GraphColorProblemBlack.png

I changed the color of all the plotlines for proper visualization.

FreeMASTER GraphColorProblemColorChanged.png

Now I selected some other Electrode for viewing purpose and now if I select the Electrode1 scope, it is again shown in black color.

Is there something which I am doing wrong.

Please help me, as I have to adjust colors every time before analyzing.

Another problem is that I have to update the micro-controller name every time in the project settings of FreeMASTER.

I am using J-Link Plus for connecting FreeMASTER with my board (no serial communication is used).

Thanks in advance.

タグ(1)
1 解決策
2,433件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

the version 3.0.3 has just been released. The issue should be fixed now.

Regards,

Michal

元の投稿で解決策を見る

3 返答(返信)
2,433件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello,

thank you for the bug report. This will be fixed in the upcoming version 3.0.3.

Regards,

Michal

2,434件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello, 

the version 3.0.3 has just been released. The issue should be fixed now.

Regards,

Michal

2,433件の閲覧回数
arun07
Contributor III

Thanks, MichalH

I just checked this today and it is working, color are now displayed.

Working.png

0 件の賞賛
返信