Compiler Warnings with "-Wpedantic"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler Warnings with "-Wpedantic"

1,670件の閲覧回数
Masmiseim
Senior Contributor I

Hello NXP team,

 

could you test the target code for Freemaster (the one running on the microcontroller) with higher warning levels and make it warning-free? May I recommend the following warning flags:

-Wall

-Wextra

-Wpedantic

 

The code raises several Compiler-Warnings with the warning-settings from above. The following three warnings, lead to linker errors when LTO is activated:

Masmiseim_0-1725635176108.png

The following linker Errors with LTO active are created when the warnings are not solved:

Masmiseim_1-1725635176109.png

Yes, at first glance these seem to have nothing to do with the warnings. It took me a while to understand the problem.

GCC13 was used on iMXRT1170.

 

Thanks and best regards

4 返答(返信)

1,072件の閲覧回数
scotty
Contributor IV

Hello @MichalH,
please can you have a look on this request. Thank you.

0 件の賞賛
返信

1,057件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Michael,

we did address most of the -Wpedantic issues in the latest version of the FreeMASTER driver. You can check the code here: https://github.com/nxp-mcuxpresso/mcux-freemaster 

We'll continue the effort in next versions.

Regards,
Michal

1,052件の閲覧回数
scotty
Contributor IV
Michal, thanks for your prompt response. I think we do not use the latest driver code from this repository right now. We will check this out.
Have a good day
michaeL
0 件の賞賛
返信

1,581件の閲覧回数
Prof_Farnsworth
Contributor I

I agree

To add to this, I also suggest to remove warnings generated with -Wundef (which seems not to be included in -Wall?)as the Freemaster header files checks a lot of potentially undefined precompiler constants.

0 件の賞賛
返信