I have installed FreeMaster 3.0 on ubuntu 18.04 and successfully done installation with inputting the Lite license. When I click FreeMASTER LITE to run it, there is not any response.
And I try to run in the terminal and I got the following error:
Cannot load library or library not found: libcll_app.so
I can find this file in the license directory.
Please advise me how to fix this problem. Thanks in advance!
Solved! Go to Solution.
Thanks. It is useful to start the freemaster lite!
And I found the solution for linux on the document getting start:
Note: on Linux machine there's an additional step required to allow the service to discover all required libraries - execute the following command before launching
node.bin:export LD_LIBRARY_PATH=$LD_LBRARY_PATH:./.
It should be run "export LD_LIBRARY_PATH=$LD_LBRARY_PATH:./" and then node.bin in its directory!
Just to generalize the correct answer: in case you are not launching FreeMASTER Lite from it's home directory or are using a link to the binary you can add the full path off the installation folder (where node.bin is stored) to LD_LIBRARY_PATH, like this:
export LD_LIBRARY_PATH=$LD_LBRARY_PATH:/path/to/FreeMASTER\ Lite
Hope this helps,
Iulian
FreeMASTER 3.0 install has two executables, FreeMASTER and FreeMASTER LITE. FreeMASTER Lite is a standalone solution that allows embedded applications compatible with NXP's FreeMASTER protocol to be monitored and controlled from ANY WEB BROWSER from a HTML5/JS web page written by the user.
The Webinar recorded very recently explains the use of Freemaster and Freemaster Lite. The Lite does not have any GUI. Please take a look. I hope this helps you.
modified by Ethan Fernandes in FreeMASTER - View the full document
Thanks. It is useful to start the freemaster lite!
And I found the solution for linux on the document getting start:
Note: on Linux machine there's an additional step required to allow the service to discover all required libraries - execute the following command before launching
node.bin:export LD_LIBRARY_PATH=$LD_LBRARY_PATH:./.
It should be run "export LD_LIBRARY_PATH=$LD_LBRARY_PATH:./" and then node.bin in its directory!