I want use freemaster in company, does it need license for company user?
Thanks.
Solved! Go to Solution.
Please mark the topic as resolved if you have no other license question.
Thanks,
Michal
Hello,
for the PC tool, I recommend to read the license terms and conditions which are available in the FreeMASTER installation as FreeMASTER-TOOL-License.pdf document, typically located in c:\NXP\FreeMASTER 3.1\FreeMASTER\license.
A similar agreement is packaged with the FreeMASTER driver code available in MCUXpresso SDK or in an installation packages available at nxp.com/freemaster.
In short, you are granted a permission to use the tool both in private or company environment only when it is used with a product using the NXP microcontroller. You can only compile and run the FreeMASTER driver code on NXP devices and you are only allowed to use the FreeMASTER PC tool to connect to NXP devices.
Regards,
Michal
Please mark the topic as resolved if you have no other license question.
Thanks,
Michal