Can FreeMASTER Lite send DTR signal for UART connection?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can FreeMASTER Lite send DTR signal for UART connection?

跳至解决方案
2,598 次查看
lucabarbiero
Contributor IV

Hello,

I want to use FreeMASTER Lite with a custom board, and establish a UART connection with the target. However my board requires the host side terminal to send Data Terminal Ready (DTR) signal.

Can the FreeMASTER Lite service issue DTR signal? This is a control signal defined in RS-232. I could not find anything the documentation.

Regards,

Luca

0 项奖励
回复
1 解答
2,558 次查看
iulian_stan
NXP Employee
NXP Employee

It will be supported on both platforms. I will DM you once we have a test build.

BR,
Iulian

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,559 次查看
lucabarbiero
Contributor IV

Hi @iulian_stan,

I would like to have this feature for both Win and Linux in the end, but I need it first and foremost for Linux. I am totally available to test it in a pre-release to help you!

0 项奖励
回复
2,559 次查看
iulian_stan
NXP Employee
NXP Employee

It will be supported on both platforms. I will DM you once we have a test build.

BR,
Iulian

0 项奖励
回复
2,583 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @lucabarbiero,

Currently, FreeMASTER Lite cannot send DTR signal.

We plan to add some control flow options in the upcoming release. I will check if DTR option will be included and will post an update in this thread.

Kind regards,
Iulian

2,565 次查看
iulian_stan
NXP Employee
NXP Employee

Update: we will support DTR.

I saw your other thread - and would like know which platform you will be using in the end. Considering DTR configuration slightly differs on Win and Unix platforms, would you be available to validate the functionality on a pre-release build ? 

0 项奖励
回复