I am porting the AN12149 ptp application note to the most recent SDK.
There are a very big differences between the fsl_enet.c FSL_ENET_DRIVER_VERSION (MAKE_VERSION(2, 3, 0)) and FSL_ENET_DRIVER_VERSION (MAKE_VERSION(2, 2, 3)), there are literally missing a lot of ieee1588 functionality like ENET_GetRxFrameTime just to mention one.
This makes it impossible to port the application.
It is somehow surprising that the library exist without being recently backwards compatible.
Do there exist any workaround to fix the incompatibility or an explanation ?
Regards Andy