Hi Guys,
Trying to bring up imx6ull via UART SDP (serial download protocol) from another imx6ull ^-^
I studied section 8.9.2 of 8.9 Serial downloader section. Got a rough idea.
Any chance who knows where we can find an example of either "command flow" or scripts in what ever language of bring up imx6ull?
Just want to fig out the exact sequence of the commands need to send to device from the host device. Like do we need to execute the dcd.bin normally etc.
Tried something like below, failed:
use 0x0A0A to write DCD.bin to device
then 0x0404 to write file to to device
jump 0x0b0b to binary start up address. but failed.
Terminal (to UART1) captures something like the attached.
Cheers,