Where is the KITPT2001SW.spi file mentioned in the KTFRDMPT2001EVMUG document?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Where is the KITPT2001SW.spi file mentioned in the KTFRDMPT2001EVMUG document?

499 次查看
zaoluo
Contributor I

I use the FRDMPT2001EVM with the marked FRDM-KL25Z board.

Where can I find the KITPT2001SW.spi file? It is shown to be located in the Injector Demo Files directory, but I can't find that directory.

thank you.

zaoluo_0-1756176617999.png

 

 

标记 (2)
0 项奖励
回复
1 回复

256 次查看
yisey
Contributor I

The KITPT2001SW.spi file comes with the SPIGen software from NXP. Install SPIGen and once installed, you will find the file in the Injector Demo Files folder inside the installation directory. For additional tips on managing files or software setups, you can also check resources like vkrenovations.ca. No download is available anywhere else, just get SPIGen from NXP.

0 项奖励
回复