Where is the KITPT2001SW.spi file mentioned in the KTFRDMPT2001EVMUG document?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the KITPT2001SW.spi file mentioned in the KTFRDMPT2001EVMUG document?

711件の閲覧回数
zaoluo
Contributor I

I use the FRDMPT2001EVM with the marked FRDM-KL25Z board.

Where can I find the KITPT2001SW.spi file? It is shown to be located in the Injector Demo Files directory, but I can't find that directory.

thank you.

zaoluo_0-1756176617999.png

 

 

タグ(2)
0 件の賞賛
返信
2 返答(返信)

468件の閲覧回数
yisey
Contributor I

The KITPT2001SW.spi file comes with the SPIGen software from NXP. Install SPIGen and once installed, you will find the file in the Injector Demo Files folder inside the installation directory. For additional tips on managing files or software setups, you can also check resources like vkrenovations.ca. No download is available anywhere else, just get SPIGen from NXP.

0 件の賞賛
返信

205件の閲覧回数
zaoluo
Contributor I

Thank you for your answer. After I downloaded and installed the SPIGen software, I didn't find the Injector Demo Files folder in the installation directory. The picture shows my installation directory. Could you instruct me on exactly where the Injector Demo Files folder or the KITPT2001SW.spi file is located?

zaoluo_0-1759919957728.png

 

0 件の賞賛
返信