RT1064 ok instead of RT1060?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1064 ok instead of RT1060?

跳至解决方案
4,755 次查看
nbgatgi
Contributor IV

I already have a few RT1064 EVKs.  Since the only significant difference that I am aware of is the 4MB of on-chip flash for the RT1064, can I use the RT1064 instead of buying the RT1060 EVK?

Update: I verified that eIQ is listed for the currently available RT1064 SDK, but it references a requirement for the RT1050 or RT1060 which apparently prevents it from being selected for inclusion with the SDK.  So a follow-up question:  Is it possible to use the RT1060 SDK with the RT1064 EVK?

1 解答
4,446 次查看
jc_pacheco
NXP Employee
NXP Employee

Hi Nick, this is under internal revision. Meanwhile, you can modify the project using the procedure described in eIQ on i.MX RT1064 EVK post.

在原帖中查看解决方案

3 回复数
4,446 次查看
jc_pacheco
NXP Employee
NXP Employee

Hi Nick,

Yes, it is possible. You could modify all memory-related MCU settings in project's properties as well as during initialization to match the FLASH on your board.

See eIQ on i.MX RT1064 EVK.

Keep in mind that support may be limited as this is not officially supported in the SDK.

0 项奖励
回复
4,446 次查看
nbgatgi
Contributor IV

Other than the internal flash of the RT1064, since there are no functional differences from the RT1060, why is it not supported?

0 项奖励
回复
4,447 次查看
jc_pacheco
NXP Employee
NXP Employee

Hi Nick, this is under internal revision. Meanwhile, you can modify the project using the procedure described in eIQ on i.MX RT1064 EVK post.