Can I Use LSDK-20.12-V5.4-RT Kernel Tag with lsdk-20.04 toolchain?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I Use LSDK-20.12-V5.4-RT Kernel Tag with lsdk-20.04 toolchain?

1,088件の閲覧回数
Wayne253
Contributor I

Hi,

 

I found that, For LSDK-20.04, only linux-4.19-rt is supported:

https://source.codeaurora.org/external/qoriq/qoriq-components/linux/tag/?h=LSDK-20.04-V4.19-RT

For LSDK-20.12, linux-5.4-rt is supported:

https://source.codeaurora.org/external/qoriq/qoriq-components/linux/tag/?h=LSDK-20.12-V5.4-RT

 

But we using LSDK-20.04 with 5.4 Kernel alredy, so can we just using LSDK-20.12-V5.4-RT Kernel Tag with lsdk-20.04 toolchain(I mean only change linux kernel source to  LSDK-20.12-V5.4-RT)

 

Many thanks.

Wayne.

タグ(2)
0 件の賞賛
返信
0 返答(返信)