When I enable adb on my AOSP 9 imx6 device, on my Linux development host this happens:
'lsusb' output on my Linux laptop connected to the device via OTG-microUSB port:
BEFORE enabling ADB on device
(base) popossri@pop-os:~/ArcX/mercury_files/manifest/jenkins/Android$ lsusb
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 003: ID 04f2:b685 Chicony Electronics Co., Ltd Chicony USB2.0 Camera
Bus 001 Device 021: ID 18d1:4ee1 Google Inc. Nexus/Pixel Device (MTP)
Bus 001 Device 004: ID 8087:0aaa Intel Corp. Bluetooth 9460/9560 Jefferson Peak (JfP)
Bus 001 Device 010: ID 0403:6001 Future Technology Devices International, Ltd FT232 Serial (UART) IC
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
AFTER enabling ADB on device
(base) popossri@pop-os:~/ArcX/mercury_files/manifest/jenkins/Android$ lsusb
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 003: ID 04f2:b685 Chicony Electronics Co., Ltd Chicony USB2.0 Camera
Bus 001 Device 004: ID 8087:0aaa Intel Corp. Bluetooth 9460/9560 Jefferson Peak (JfP)
Bus 001 Device 010: ID 0403:6001 Future Technology Devices International, Ltd FT232 Serial (UART) IC
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
On my Samsung phone, I have to enable USB debugging using special instructions before it can be used by ADB. I tried doing that by changing device.mk so that my /system/build.prop has the following entries:
persist.service.adb.enable=1
persist.service.debuggable=1
persist.sys.usb.config=mtp,adb
But the device doesn't show up in 'adb devices' .
TCP(ethernet) based adb connection works just fine.What else should I check and enable?
解決済! 解決策の投稿を見る。
It turned out that the serial number ro.serialno was not passed in as kernel command line argument. Once that was fixed in BoardConfig.mk, ADB over USB worked and the device showed up on both Linux and Windows hosts.
Based on what I read on other stackoverflow posts , I have enabled these properties:
:/ # getprop **persist.sys.usb.config ptp,adb** :/ # getprop | grep usb [init.svc.usb-hal-1-1]: [running] [init.svc.usbd]: [stopped] [persist.sys.usb.config]: [ptp,adb] [ro.boottime.usb-hal-1-1]: [11083523334] [ro.boottime.usbd]: [11451505001] **[sys.usb.config]: [ptp,adb]** [sys.usb.configfs]: [2] [sys.usb.controller]: [ci_hdrc.0] [sys.usb.ffs.ready]: [0] [sys.usb.mtp.device_type]: [3] **[service.adb.tcp.port]: [-1]** [vendor.usb.config]: [ci_hdrc.0]
Also, I have enabled 'USB debugging' in developer settings. But despite setting [sys.oem_unlock_allowed]: [1], I could not enable OEM unlocking'. Perhaps its because we're using a custom bootloader, not U-boot?
Finally, adb devices -l on a Ubuntu host connected to the device does not list the AOSP9 device and ADB over USB hasn't worked so far.
What can I try next to resolve this?