whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

3,008 次查看
terrybogard
Contributor II

whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

0 项奖励
回复
3 回复数

3,007 次查看
KalaimaniArumugam
Contributor III

terrybogard,

     MC56f82748 GPIOD4 ResetB is a 3.3Volt level pin and it mentioned in technical datasheet chapter"11.1 Signal Multiplexing and Pin Assignments"

0 项奖励
回复

3,005 次查看
terrybogard
Contributor II

maybe this means the pin can't set 5V like other GPIO pins. Or this mean if resetB is below 3.3v, the external reset will  happen?

0 项奖励
回复

3,003 次查看
KalaimaniArumugam
Contributor III

terrybogard,

RESETB only operated in 3.3Volts that also mentioned in Datasheet(Page 2). You Can refer the image.

0 项奖励
回复