whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

1,591 Views
terrybogard
Contributor II

whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

0 Kudos
3 Replies

1,590 Views
KalaimaniArumugam
Contributor III

terrybogard,

     MC56f82748 GPIOD4 ResetB is a 3.3Volt level pin and it mentioned in technical datasheet chapter"11.1 Signal Multiplexing and Pin Assignments"

0 Kudos

1,588 Views
terrybogard
Contributor II

maybe this means the pin can't set 5V like other GPIO pins. Or this mean if resetB is below 3.3v, the external reset will  happen?

0 Kudos

1,586 Views
KalaimaniArumugam
Contributor III

terrybogard,

RESETB only operated in 3.3Volts that also mentioned in Datasheet(Page 2). You Can refer the image.

0 Kudos