whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

2,570件の閲覧回数
terrybogard
Contributor II

whtat's the voltage level of MC56f82748 GPIOD4 ResetB will trigger external reset?

0 件の賞賛
返信
3 返答(返信)

2,569件の閲覧回数
KalaimaniArumugam
Contributor III

terrybogard,

     MC56f82748 GPIOD4 ResetB is a 3.3Volt level pin and it mentioned in technical datasheet chapter"11.1 Signal Multiplexing and Pin Assignments"

0 件の賞賛
返信

2,567件の閲覧回数
terrybogard
Contributor II

maybe this means the pin can't set 5V like other GPIO pins. Or this mean if resetB is below 3.3v, the external reset will  happen?

0 件の賞賛
返信

2,565件の閲覧回数
KalaimaniArumugam
Contributor III

terrybogard,

RESETB only operated in 3.3Volts that also mentioned in Datasheet(Page 2). You Can refer the image.

0 件の賞賛
返信