Write Protection of the EFlex PWM Module in DSC84xxx and DSC827xx Families

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Write Protection of the EFlex PWM Module in DSC84xxx and DSC827xx Families

ソリューションへジャンプ
1,655件の閲覧回数
GottiLuca
Contributor IV

I've noticed that in this module ( Enhanced Flexible PWM ) there aren't write protected registers, in particular for the safety relevant registers ( i.e. : PWMA_SMnDISMAP0-1 which enable/disable the fault protection ).

 

I would like to have an explanation about this choice since on the PWM Modules of previous DSC families ( like DSC803-2x or DSC83xx ) such possibility was always included .

 

To my opinion, this is a quite important missed feature for a PWM module ..

 

If, on the other hand, there is a way to write-protect the PWM safety registers, let me know how .

ラベル(1)
0 件の賞賛
返信
1 解決策
1,373件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Luca,

yes, you are right, the Enhanced Flexible PWM module does not support safety mode, all register can be modified anytime without write-protection.

BR

XiangJun Rong.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,374件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Luca,

yes, you are right, the Enhanced Flexible PWM module does not support safety mode, all register can be modified anytime without write-protection.

BR

XiangJun Rong.

0 件の賞賛
返信