Where can I obtain the source codes of the GPLv2 tools used in Symphony Studio (custom OpenOCD, GDB, GCC, GDBSIM) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I obtain the source codes of the GPLv2 tools used in Symphony Studio (custom OpenOCD, GDB, GCC, GDBSIM) ?

880件の閲覧回数
matesebok
Contributor I

Also looked in the Eclipse license, it should be available too in a "reasonable manner".

In the readme there is the following:

4. Licensing
================================================================================

This release contains as-yet-unreleased modifications to open source software
that are the property of Freescale Semiconductor Inc. All sources bound by the
GNU General Public License can be obtained by lodging a written request to
Freescale Semiconductor Inc.

But after multiple attempt to ask by email I just got nonsense responses.

These are legacy tools for legacy components.
Please make them public for research and to contribute to the open source community your tools are derivative of.

0 件の賞賛
返信
0 返答(返信)