TJA1057GTK/3Z EMC issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1057GTK/3Z EMC issue

ソリューションへジャンプ
1,538件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,

I've got an EMC issue with the TJA1057GTK/3Z. The CAN transceiver will sometimes be destroyed at EMC test when I apply 100V/m in a GTEM cell.

Does someone know this issue? Does someone have a workaround?

 

Regards.

Boris_Bloxsberg_0-1645084951695.png

 

 

 

0 件の賞賛
返信
1 解決策
1,511件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please read attached file and modify circuit for enhance the EMC performance.

元の投稿で解決策を見る

3 返答(返信)
1,512件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please read attached file and modify circuit for enhance the EMC performance.

1,528件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please give more information for your said ---destroyed at EMC test when I apply 100V/m in a GTEM cell.

How to destroy it? the part damaged? what does mean about 100V/m in GTEM cell?

0 件の賞賛
返信
1,524件の閲覧回数
Boris_Bloxsberg
Contributor III

Hi,

when I apply 100 Volts pre meter field strength to the transceiver, the transceiver will be destroyed. That means the transceiver does not transmit any can messages and the current consumption of the transceiver is higher than normal.

If I replace the transceiver with a new one. Everything is fine and the circuit is working

Regards.

 

0 件の賞賛
返信