TEA2017 start up issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA2017 start up issues

2,054 Views
Maxjay
Contributor II

Customer is working on the 150W design (24V/6.25A) now, but currently facing start up when output current is 3A (the pin 15 will be trigger), 2A/4A is normal operation, any idea for this issues? Below is start up waveform Screenshot 2025-03-11 230029.png

0 Kudos
Reply
2 Replies

1,331 Views
james698goff
Contributor I

Hello,
The issue at 3A startup may be due to SNSCURLLC triggering prematurely—TEA2017 allows this during startup to avoid false OCP. Verify your schematic using the TEA2017 design tool and check if the calculation sheet parameters align with expected startup behavior. Adjusting soft-start or current sense thresholds may help stabilize the 3A condition.

Best Regards,
James Goff

0 Kudos
Reply

2,022 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi Maxjay

1:代理商的问题我们建议直接提ticket。

这里还是建议客户先用calcualtion sheet核实原理图

2:

在启动的时候是允许SNSCURLLC有动作的是为了防止触发OCP/

0 Kudos
Reply