SC18IS606 puts 1 in every 7e bit of a byte

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IS606 puts 1 in every 7e bit of a byte

Jump to solution
2,919 Views
DannyEngeringh
Contributor III

Hello everyone, 

I'm trying to use a SC18IS606 incombination with a BGT60UTR. Writing the registers seems to work. but when i try to read back the register values. the SC18IS606 puts a one in every 7e bit of a byte. On the logic analyzer I see the right values coming by. but reading them seems not to work properly. 

I hope somebody can help. 

Regards

Tags (1)
0 Kudos
Reply
1 Solution
2,890 Views
DannyEngeringh
Contributor III

Hi guoweisun, 

Thanks for your reply, The problem was caused by my raspberry-pi. do not realy understand why but with a different processor the problem was solved. 

regards

View solution in original post

0 Kudos
Reply
2 Replies
2,894 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI Danny:

Thanks for your interest in NXP  Products.

You can see below read command format:

guoweisun_0-1731563793086.png

guoweisun_2-1731564445507.png

 

You can see above read command for instance.

Thanks!

 

 

0 Kudos
Reply
2,891 Views
DannyEngeringh
Contributor III

Hi guoweisun, 

Thanks for your reply, The problem was caused by my raspberry-pi. do not realy understand why but with a different processor the problem was solved. 

regards

0 Kudos
Reply