Quadrature pulse output generation with MC56F827 controller.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Quadrature pulse output generation with MC56F827 controller.

ソリューションへジャンプ
2,104件の閲覧回数
manikandanb
Contributor II

Hello all,

I need to generate the quadrature pulse (each with 90degree displacement) like the motor encoder signals. How to generate this with eFlex PWM in MC56F8247 microcontroller. What configuration should I made for this..??

I am using codeWarrior v10.6

Can anyone help me out for solving this.

 

Thanks in advance.

0 件の賞賛
返信
1 解決策
2,091件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the eFlexPWM module supports phase shift feature, so it i okay to generate the phase shift signals to simulate the PH_A and PH_B signal with PWM output signals.

I attach the example based on MC56F84789, pls refer to it.

BR

XiangJun Rong

元の投稿で解決策を見る

2 返答(返信)
2,092件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the eFlexPWM module supports phase shift feature, so it i okay to generate the phase shift signals to simulate the PH_A and PH_B signal with PWM output signals.

I attach the example based on MC56F84789, pls refer to it.

BR

XiangJun Rong

2,086件の閲覧回数
manikandanb
Contributor II

Thanks for your response,

I will check the code.

0 件の賞賛
返信